Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
Modifier and Type | Field and Description |
---|---|
static Measurement.DeviationReportType |
Measurement.DeviationReportType.ALL_DEVIATION
All Deviation
|
static Measurement.DeviationReportType |
Measurement.DeviationReportType.MAXIMUM_ANGLE
Maximum Angle
|
static Measurement.DeviationReportType |
Measurement.DeviationReportType.MAXIMUM_DISTANCE
Maximum Distance
|
static Measurement.DeviationReportType |
Measurement.DeviationReportType.MINIMUM_ANGLE
Minimum Angle
|
static Measurement.DeviationReportType |
Measurement.DeviationReportType.MINIMUM_DISTANCE
Minimum Distance
|
static Measurement.DeviationReportType |
Measurement.DeviationReportType.NO_DEVIATION
No Deviation
|
Modifier and Type | Method and Description |
---|---|
static Measurement.DeviationReportType |
Measurement.DeviationReportType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static Measurement.DeviationReportType |
Measurement.DeviationReportType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static Measurement.DeviationReportType[] |
Measurement.DeviationReportType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
Measurement.displayDeviationChecking(Curve curve1,
Face face2,
int numOfCheckPoints,
double distanceTolerance,
double angularTolerance,
Measurement.DeviationReportType reportType)
Checks deviations between a curve and a face (curve to face), and displays the report.
|
void |
Measurement.displayDeviationChecking(Face face1,
Edge edge1,
Face face2,
Edge edge2,
int numOfCheckPoints,
double distanceTolerance,
double angularTolerance,
Measurement.DeviationReportType reportType)
Checks deviations between edges (edge to edge), and displays the report.
|
void |
Measurement.displayDeviationChecking(Face face1,
Edge edge1,
Face face2,
int numOfCheckPoints,
double distanceTolerance,
double angularTolerance,
Measurement.DeviationReportType reportType)
Checks deviations between a edge and a face (edge to face), and displays the report.
|
void |
Measurement.displayDeviationChecking(Face face1,
Face face2,
int numOfCheckPointsU,
int numOfCheckPointsV,
double distanceTolerance,
double angularTolerance,
Measurement.DeviationReportType reportType)
Checks deviations between faces (face to face), and displays the report.
|
void |
Measurement.displayDeviationChecking(ICurve curve1,
ICurve curve2,
int numOfCheckPoints,
double distanceTolerance,
double angularTolerance,
Measurement.DeviationReportType reportType)
Checks deviations between curves (curve to curve),and displays the report.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.