Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
nxopen.routing |
Provides classes and interfaces for Routing.
|
Modifier and Type | Method and Description |
---|---|
MeasureDistanceBuilder |
MeasureManager.createMeasureDistanceBuilder(NXObject feature)
Creates a
MeasureDistanceBuilder
Note: This class is used internally for measurement, but is not required for creation
of a distance measurement. |
Modifier and Type | Method and Description |
---|---|
RoutingMeasureDistanceBuilder |
MeasureManager.createRoutingMeasureDistanceBuilder(NXObject feature,
MeasureDistanceBuilder measureDistanceBuilder)
Creates a
RoutingMeasureDistanceBuilder
It inherits the properties from MeasureDistanceBuilder and destroys it. |
Modifier and Type | Interface and Description |
---|---|
interface |
RoutingMeasureDistanceBuilder
Represents a
RoutingMeasureDistanceBuilder Creator not available in KF because transient objects are not supported. |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.