Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
Modifier and Type | Field and Description |
---|---|
static MeasureDistanceBuilder.MeasureType |
MeasureDistanceBuilder.MeasureType.LOCAL_MINIMUM |
static MeasureDistanceBuilder.MeasureType |
MeasureDistanceBuilder.MeasureType.MAX_CLEARANCE |
static MeasureDistanceBuilder.MeasureType |
MeasureDistanceBuilder.MeasureType.MAXIMUM |
static MeasureDistanceBuilder.MeasureType |
MeasureDistanceBuilder.MeasureType.MIN_CLEARANCE |
static MeasureDistanceBuilder.MeasureType |
MeasureDistanceBuilder.MeasureType.MINIMUM |
static MeasureDistanceBuilder.MeasureType |
MeasureDistanceBuilder.MeasureType.TO_APOINT |
Modifier and Type | Method and Description |
---|---|
MeasureDistanceBuilder.MeasureType |
MeasureDistanceBuilder.mtype()
Returns the mtype
License requirements: None. |
static MeasureDistanceBuilder.MeasureType |
MeasureDistanceBuilder.MeasureType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static MeasureDistanceBuilder.MeasureType |
MeasureDistanceBuilder.MeasureType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static MeasureDistanceBuilder.MeasureType[] |
MeasureDistanceBuilder.MeasureType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
MeasureDistanceBuilder.setMtype(MeasureDistanceBuilder.MeasureType mtype)
License requirements: solid_modeling ("SOLIDS MODELING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.