Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
Modifier and Type | Field and Description |
---|---|
static MeasureBodies.AnalysisUnit |
MeasureBodies.AnalysisUnit.CUSTOM_UNIT |
static MeasureBodies.AnalysisUnit |
MeasureBodies.AnalysisUnit.GRAM_CENTIMETER |
static MeasureBodies.AnalysisUnit |
MeasureBodies.AnalysisUnit.GRAM_MILLIMETER |
static MeasureBodies.AnalysisUnit |
MeasureBodies.AnalysisUnit.KILOGRAM_METER |
static MeasureBodies.AnalysisUnit |
MeasureBodies.AnalysisUnit.KILOGRAM_MILLIMETER |
static MeasureBodies.AnalysisUnit |
MeasureBodies.AnalysisUnit.POUND_FOOT |
static MeasureBodies.AnalysisUnit |
MeasureBodies.AnalysisUnit.POUND_INCH |
Modifier and Type | Method and Description |
---|---|
MeasureBodies.AnalysisUnit |
MeasureBodies.informationUnit()
Returns the family of units for mass properties in the information window
License requirements: None. |
static MeasureBodies.AnalysisUnit |
MeasureBodies.AnalysisUnit.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static MeasureBodies.AnalysisUnit |
MeasureBodies.AnalysisUnit.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static MeasureBodies.AnalysisUnit[] |
MeasureBodies.AnalysisUnit.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
MeasureBodies.setInformationUnit(MeasureBodies.AnalysisUnit unitValue)
License requirements: None. |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.