Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
Modifier and Type | Field and Description |
---|---|
static MeasureAngleBuilder.OrientationType |
MeasureAngleBuilder.OrientationType.INNER_ANGLE |
static MeasureAngleBuilder.OrientationType |
MeasureAngleBuilder.OrientationType.OUTER_ANGLE |
Modifier and Type | Method and Description |
---|---|
MeasureAngleBuilder.OrientationType |
MeasureAngleBuilder.orientation()
Returns the orientation
License requirements: None. |
static MeasureAngleBuilder.OrientationType |
MeasureAngleBuilder.OrientationType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static MeasureAngleBuilder.OrientationType |
MeasureAngleBuilder.OrientationType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static MeasureAngleBuilder.OrientationType[] |
MeasureAngleBuilder.OrientationType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
MeasureAngleBuilder.setOrientation(MeasureAngleBuilder.OrientationType mtype)
License requirements: solid_modeling ("SOLIDS MODELING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.