Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
Modifier and Type | Field and Description |
---|---|
static LoadOptions.UpdateSubsetOnLoad |
LoadOptions.UpdateSubsetOnLoad.NONE
replay recipe
|
static LoadOptions.UpdateSubsetOnLoad |
LoadOptions.UpdateSubsetOnLoad.REPLAY_RECIPE
do not update
|
Modifier and Type | Method and Description |
---|---|
LoadOptions.UpdateSubsetOnLoad |
LoadOptions.optionUpdateSubsetOnLoad()
Returns the option that controls the subset updates during load
License requirements: None. |
static LoadOptions.UpdateSubsetOnLoad |
LoadOptions.UpdateSubsetOnLoad.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static LoadOptions.UpdateSubsetOnLoad |
LoadOptions.UpdateSubsetOnLoad.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static LoadOptions.UpdateSubsetOnLoad[] |
LoadOptions.UpdateSubsetOnLoad.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
LoadOptions.setOptionUpdateSubsetOnLoad(LoadOptions.UpdateSubsetOnLoad option)
Sets the option that controls the subset updates during load
License requirements: None. |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.