Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
Modifier and Type | Field and Description |
---|---|
static LoadOptions.LoadOption |
LoadOptions.LoadOption.FULLY_LOAD
partial load : off, use lightweight : off
|
static LoadOptions.LoadOption |
LoadOptions.LoadOption.FULLY_LOAD_LIGHTWEIGHT_DISPLAY
partial load : off, use lightweight : on
|
static LoadOptions.LoadOption |
LoadOptions.LoadOption.MINIMAL_LOAD_VISUALIZE
reserved for future use
|
static LoadOptions.LoadOption |
LoadOptions.LoadOption.PARTIALLY_LOAD
partial load : on, use lightweight : off
|
static LoadOptions.LoadOption |
LoadOptions.LoadOption.PARTIALLY_LOAD_LIGHTWEIGHT_DISPLAY
partial load : on, use lightweight : on
|
Modifier and Type | Method and Description |
---|---|
LoadOptions.LoadOption |
LoadOptions.partLoadOption()
Returns the option that controls how the part is being loaded
License requirements: assemblies ("ASSEMBLIES MODULE") . |
static LoadOptions.LoadOption |
LoadOptions.LoadOption.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static LoadOptions.LoadOption |
LoadOptions.LoadOption.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static LoadOptions.LoadOption[] |
LoadOptions.LoadOption.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
LoadOptions.setPartLoadOption(LoadOptions.LoadOption loadOption)
Sets the option that controls how the part is being loaded
License requirements: assemblies ("ASSEMBLIES MODULE") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.