Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
Modifier and Type | Field and Description |
---|---|
static LoadOptions.BookmarkRefsets |
LoadOptions.BookmarkRefsets.DONT_IMPORT
Do nothing with the bookmark reference set data
|
static LoadOptions.BookmarkRefsets |
LoadOptions.BookmarkRefsets.IMPORT_AND_OPTIMIZE_LOAD
Import reference set data and use it to optimize load
|
static LoadOptions.BookmarkRefsets |
LoadOptions.BookmarkRefsets.IMPORT_DATA
Import reference set data
|
Modifier and Type | Method and Description |
---|---|
LoadOptions.BookmarkRefsets |
LoadOptions.bookmarkRefsetLoadBehavior()
Returns the options that specify import and loading of components' reference sets when opening bookmarks.
|
static LoadOptions.BookmarkRefsets |
LoadOptions.BookmarkRefsets.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static LoadOptions.BookmarkRefsets |
LoadOptions.BookmarkRefsets.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static LoadOptions.BookmarkRefsets[] |
LoadOptions.BookmarkRefsets.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
LoadOptions.setBookmarkRefsetLoadBehavior(LoadOptions.BookmarkRefsets refsetLoadOption)
Sets the options that specify import and loading of components' reference sets when opening bookmarks.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.