Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
Modifier and Type | Field and Description |
---|---|
LoadOptions.BookmarkComponents |
LoadOptions.BookmarkComponentsToLoadData.componentsLoadOption
what components to load
|
static LoadOptions.BookmarkComponents |
LoadOptions.BookmarkComponents.LOAD_LOADED
Load and show only what was loaded on the bookmark's save
Load invisible components and keep them invisible.
|
static LoadOptions.BookmarkComponents |
LoadOptions.BookmarkComponents.LOAD_LOADED_AND_NON_DISPLAYED
Load and show only what was loaded on the bookmark's save, including non-display parts.
|
static LoadOptions.BookmarkComponents |
LoadOptions.BookmarkComponents.LOAD_VISIBLE
Load and show only what was shown on the bookmark's save.
|
static LoadOptions.BookmarkComponents |
LoadOptions.BookmarkComponents.NO_CHANGE
This option has no effect.
|
Modifier and Type | Method and Description |
---|---|
static LoadOptions.BookmarkComponents |
LoadOptions.BookmarkComponents.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static LoadOptions.BookmarkComponents |
LoadOptions.BookmarkComponents.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static LoadOptions.BookmarkComponents[] |
LoadOptions.BookmarkComponents.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
LoadOptions.setBookmarkComponentsToLoad(boolean restoreAnt,
boolean restoreFullyLoadedStatus,
LoadOptions.BookmarkComponents componentsLoadOption)
License requirements: None. |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.