Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
Modifier and Type | Field and Description |
---|---|
static LineWidthOption |
LineWidthOption.ASSIGNED
Width value can be obtained from the builder.
|
static LineWidthOption |
LineWidthOption.DEFAULT
Default width.
|
static LineWidthOption |
LineWidthOption.NO_CHANGE
Do not modify the width.
|
Modifier and Type | Method and Description |
---|---|
static LineWidthOption |
LineWidthOption.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static LineWidthOption |
LineWidthOption.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static LineWidthOption[] |
LineWidthOption.values()
Returns an array that contains the values for this enum.
|
LineWidthOption |
LineWidthBuilder.widthOption()
Returns the width option
Use LineWidthBuilder.isValidOption(nxopen.LineWidthOption)
to check whether the width option is supported by the builder. |
Modifier and Type | Method and Description |
---|---|
boolean |
LineWidthBuilder.isValidOption(LineWidthOption widthOption)
Determines if the specified width option is supported.
|
void |
LineWidthBuilder.setWidthOption(LineWidthOption widthOption)
License requirements: None. |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.