Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
Modifier and Type | Field and Description |
---|---|
static LayoutDefinition.ArrangementType |
LayoutDefinition.ArrangementType.L1
One row by one column
|
static LayoutDefinition.ArrangementType |
LayoutDefinition.ArrangementType.L2
One row by two columns
|
static LayoutDefinition.ArrangementType |
LayoutDefinition.ArrangementType.L3
Two rows by one column
|
static LayoutDefinition.ArrangementType |
LayoutDefinition.ArrangementType.L4
Two rows by two columns
|
static LayoutDefinition.ArrangementType |
LayoutDefinition.ArrangementType.L6
Two rows by three columns
|
static LayoutDefinition.ArrangementType |
LayoutDefinition.ArrangementType.L9
Three rows by three columns
|
static LayoutDefinition.ArrangementType |
LayoutDefinition.ArrangementType.NON_STANDARD
A non standard layout.
|
Modifier and Type | Method and Description |
---|---|
LayoutDefinition.ArrangementType |
LayoutDefinition.arrangement()
Returns the arrangement type of the layout definition.
|
static LayoutDefinition.ArrangementType |
LayoutDefinition.ArrangementType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static LayoutDefinition.ArrangementType |
LayoutDefinition.ArrangementType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static LayoutDefinition.ArrangementType[] |
LayoutDefinition.ArrangementType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
LayoutDefinition |
LayoutCollection.newLayoutDefinition(LayoutDefinition.ArrangementType arrangement)
Constructs a
LayoutDefinition object to be used to create a layout. |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.