Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
Modifier and Type | Interface and Description |
---|---|
interface |
SketchHelpedDimensionalConstraint
Represents a dimensional sketch constraint that has a help point or help parameter
. |
interface |
SketchHelpedGeometricConstraint
Represents a geometric sketch constraint that has a help point or help parameter
To obtain an instance of this class, use Sketch . |
interface |
SketchTangentConstraint
Represents a tangent constraint
To create an instance of this object use Sketch.createTangentConstraint(nxopen.Sketch.ConstraintGeometry, nxopen.Sketch.ConstraintGeometryHelp, nxopen.Sketch.ConstraintGeometry, nxopen.Sketch.ConstraintGeometryHelp) Created in NX3.0.0 |
interface |
SketchTangentToStringConstraint
Represents a sketch tangent to string constraint
Use SketchCollection.createConstraintBuilder() to create an instance of this class. |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.