Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
nxopen.die |
Provides classes and interfaces relating to Die Engineering and Die Design.
|
nxopen.drawings |
Provides classes and interfaces for Drafting Drawings.
|
Modifier and Type | Interface and Description |
---|---|
interface |
Body
Represents a Body
.
|
interface |
CartesianCoordinateSystem
Represents a cartesian coordinate system
To create a new instance of this class, use CoordinateSystemCollection.createCoordinateSystem(nxopen.Point3d, nxopen.Matrix3x3, boolean) Created in NX4.0.0 |
interface |
CoordinateSystem
Represents a coordinate system
This is an abstract class . |
interface |
CylindricalCoordinateSystem
Represents a cylindrical coordinate system
To create a new instance of this class, use CoordinateSystemCollection.createCylindricalCoordinateSystem(nxopen.Point3d, nxopen.Vector3d, nxopen.Vector3d) Created in NX4.0.0 |
interface |
DatumAxis
Represents a datum axis
This object can not be created by KF it's the display objet of the datum axis . |
interface |
DatumPlane
Represents a datum plane
This object can not be created by KF it's the display objet of the datum plane . |
interface |
Face
Represents a face .
|
interface |
Plane
Represents an
Plane class. |
interface |
Point
Represents a smart
Point . |
interface |
SphericalCoordinateSystem
Represents a spherical coordinate system
To create a new instance of this class, use CoordinateSystemCollection.createSphericalCoordinateSystem(nxopen.Point3d, nxopen.Vector3d, nxopen.Vector3d) Created in NX4.0.0 |
Modifier and Type | Interface and Description |
---|---|
interface |
MeshPoint
Represents a smart
MeshPoint . |
Modifier and Type | Method and Description |
---|---|
IOrientation |
RibChildBuilder.bottom()
Returns the bottom limit geometry of the die rib.
|
IOrientation |
RibChildBuilder.bottomEnd()
Returns the bottom end limit geometry of the die rib.
|
IOrientation |
DrawDiePunchBuilder.closedStartOrientation()
Returns the closed start orientation of the draw die punch casting.
|
IOrientation |
PadChildBuilder.limitingSurface()
Returns the limiting surface of the die pad.
|
IOrientation |
PadChildBuilder.orientationPlane()
Returns the orientation plane of the die pad.
|
IOrientation |
KeywayChildBuilder.plane()
Returns the plane of the keyway.
|
IOrientation |
SteelInsertSegmentChildBuilder.segPoint()
Returns the steel insert seg point or plane
License requirements: ug_die_design ("Die Design") . |
IOrientation |
RibChildBuilder.start()
Returns the start limit geometry of the die rib.
|
IOrientation |
RibChildBuilder.top()
Returns the top limit geometry of the die rib.
|
IOrientation |
RibChildBuilder.topEnd()
Returns the top end limit geometry of the die rib.
|
Modifier and Type | Method and Description |
---|---|
void |
RibChildBuilder.setBottom(IOrientation bottom)
Sets the bottom limit geometry of the die rib.
|
void |
RibChildBuilder.setBottomEnd(IOrientation bottomEnd)
Sets the bottom end limit geometry of the die rib.
|
void |
DrawDiePunchBuilder.setClosedStartOrientation(IOrientation closedStartOrientation)
Sets the closed start orientation of the draw die punch casting.
|
void |
PadChildBuilder.setLimitingSurface(IOrientation limitingSurface)
Sets the limiting surface of the die pad.
|
void |
PadChildBuilder.setOrientationPlane(IOrientation orientationPlane)
Sets the orientation plane of the die pad.
|
void |
KeywayChildBuilder.setPlane(IOrientation plane)
Sets the plane of the keyway.
|
void |
SteelInsertSegmentChildBuilder.setSegPoint(IOrientation segPoint)
Sets the steel insert seg point or plane
License requirements: ug_die_design ("Die Design") . |
void |
RibChildBuilder.setStart(IOrientation start)
Sets the start limit geometry of the die rib.
|
void |
RibChildBuilder.setTop(IOrientation top)
Sets the top limit geometry of the die rib.
|
void |
RibChildBuilder.setTopEnd(IOrientation topEnd)
Sets the top end limit geometry of the die rib.
|
Modifier and Type | Interface and Description |
---|---|
interface |
DraftingPoint
Represents a Drafting VD Point.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.