Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
Modifier and Type | Field and Description |
---|---|
static HumanPosturePredictionBuilder.VehicleType |
HumanPosturePredictionBuilder.VehicleType.CLASS_A
Indicate Class A vehicle.
|
static HumanPosturePredictionBuilder.VehicleType |
HumanPosturePredictionBuilder.VehicleType.CLASS_B
Indicate Class B vehicle.
|
static HumanPosturePredictionBuilder.VehicleType |
HumanPosturePredictionBuilder.VehicleType.CLASS_SEATED_SOLDIER
Seated soldier
|
Modifier and Type | Method and Description |
---|---|
static HumanPosturePredictionBuilder.VehicleType |
HumanPosturePredictionBuilder.VehicleType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static HumanPosturePredictionBuilder.VehicleType |
HumanPosturePredictionBuilder.VehicleType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static HumanPosturePredictionBuilder.VehicleType[] |
HumanPosturePredictionBuilder.VehicleType.values()
Returns an array that contains the values for this enum.
|
HumanPosturePredictionBuilder.VehicleType |
HumanPosturePredictionBuilder.vehicle()
Returns the vehicle type: Class A, Class B or Seated Soldier
License requirements: solid_modeling ("SOLIDS MODELING"), ug_human ("Human Modelling") . |
Modifier and Type | Method and Description |
---|---|
void |
HumanPosturePredictionBuilder.setVehicle(HumanPosturePredictionBuilder.VehicleType vehicleType)
License requirements: solid_modeling ("SOLIDS MODELING"), ug_human ("Human Modelling") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.