Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
Modifier and Type | Field and Description |
---|---|
static HumanPosturePredictionBuilder.TransmissionType |
HumanPosturePredictionBuilder.TransmissionType.AUTOMATIC
Indicate automatic transmission
|
static HumanPosturePredictionBuilder.TransmissionType |
HumanPosturePredictionBuilder.TransmissionType.MANUAL
Indicate manual transmission
|
Modifier and Type | Method and Description |
---|---|
HumanPosturePredictionBuilder.TransmissionType |
HumanPosturePredictionBuilder.transmission()
Returns the transmission type: automatic or manual.
|
static HumanPosturePredictionBuilder.TransmissionType |
HumanPosturePredictionBuilder.TransmissionType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static HumanPosturePredictionBuilder.TransmissionType |
HumanPosturePredictionBuilder.TransmissionType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static HumanPosturePredictionBuilder.TransmissionType[] |
HumanPosturePredictionBuilder.TransmissionType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
HumanPosturePredictionBuilder.setTransmission(HumanPosturePredictionBuilder.TransmissionType transmissionType)
License requirements: solid_modeling ("SOLIDS MODELING"), ug_human ("Human Modelling") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.