Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
Modifier and Type | Field and Description |
---|---|
static HumanPosturePredictionBuilder.SeatType |
HumanPosturePredictionBuilder.SeatType.ADJUSTABLE
Indicate adjustable seat
|
static HumanPosturePredictionBuilder.SeatType |
HumanPosturePredictionBuilder.SeatType.FIXED
Indicate fixed seat
|
Modifier and Type | Method and Description |
---|---|
HumanPosturePredictionBuilder.SeatType |
HumanPosturePredictionBuilder.seat()
Returns the seat type: fixed seat or adjustable seat
License requirements: solid_modeling ("SOLIDS MODELING"), ug_human ("Human Modelling") . |
static HumanPosturePredictionBuilder.SeatType |
HumanPosturePredictionBuilder.SeatType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static HumanPosturePredictionBuilder.SeatType |
HumanPosturePredictionBuilder.SeatType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static HumanPosturePredictionBuilder.SeatType[] |
HumanPosturePredictionBuilder.SeatType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
HumanPosturePredictionBuilder.setSeat(HumanPosturePredictionBuilder.SeatType seatType)
License requirements: solid_modeling ("SOLIDS MODELING"), ug_human ("Human Modelling") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.