Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
Modifier and Type | Field and Description |
---|---|
static HumanPosturePredictionBuilder.PredictionMethodType |
HumanPosturePredictionBuilder.PredictionMethodType.ASPECT
Indicate ASPECT H_point method
|
static HumanPosturePredictionBuilder.PredictionMethodType |
HumanPosturePredictionBuilder.PredictionMethodType.PRE_ASPECT
Indicate Pre-ASPECT H_point method
|
Modifier and Type | Method and Description |
---|---|
HumanPosturePredictionBuilder.PredictionMethodType |
HumanPosturePredictionBuilder.predictionMethod()
Returns the prediction method: aspect or pre_aspect
License requirements: solid_modeling ("SOLIDS MODELING"), ug_human ("Human Modelling") . |
static HumanPosturePredictionBuilder.PredictionMethodType |
HumanPosturePredictionBuilder.PredictionMethodType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static HumanPosturePredictionBuilder.PredictionMethodType |
HumanPosturePredictionBuilder.PredictionMethodType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static HumanPosturePredictionBuilder.PredictionMethodType[] |
HumanPosturePredictionBuilder.PredictionMethodType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
HumanPosturePredictionBuilder.setPredictionMethod(HumanPosturePredictionBuilder.PredictionMethodType predictionMethodType)
License requirements: solid_modeling ("SOLIDS MODELING"), ug_human ("Human Modelling") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.