Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
Modifier and Type | Field and Description |
---|---|
static HumanPosturePredictionBuilder.CushionFirmnessType |
HumanPosturePredictionBuilder.CushionFirmnessType.FIRM
Indicate firm cushion
|
static HumanPosturePredictionBuilder.CushionFirmnessType |
HumanPosturePredictionBuilder.CushionFirmnessType.MEDIUM
Indicate medium cushion
|
static HumanPosturePredictionBuilder.CushionFirmnessType |
HumanPosturePredictionBuilder.CushionFirmnessType.SOFT
Indicate soft cushion
|
Modifier and Type | Method and Description |
---|---|
HumanPosturePredictionBuilder.CushionFirmnessType |
HumanPosturePredictionBuilder.cushionFirmness()
Returns the cushion firmness type: soft cushion, medium cushion or firm cushion
License requirements: solid_modeling ("SOLIDS MODELING"), ug_human ("Human Modelling") . |
static HumanPosturePredictionBuilder.CushionFirmnessType |
HumanPosturePredictionBuilder.CushionFirmnessType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static HumanPosturePredictionBuilder.CushionFirmnessType |
HumanPosturePredictionBuilder.CushionFirmnessType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static HumanPosturePredictionBuilder.CushionFirmnessType[] |
HumanPosturePredictionBuilder.CushionFirmnessType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
HumanPosturePredictionBuilder.setCushionFirmness(HumanPosturePredictionBuilder.CushionFirmnessType cushionFirmnessType)
License requirements: solid_modeling ("SOLIDS MODELING"), ug_human ("Human Modelling") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.