Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
Modifier and Type | Field and Description |
---|---|
static HumanData.HandFootType |
HumanData.HandFootType.FOOT
Indicate the foot
|
static HumanData.HandFootType |
HumanData.HandFootType.HAND
Indicate the hand
|
Modifier and Type | Method and Description |
---|---|
static HumanData.HandFootType |
HumanData.HandFootType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static HumanData.HandFootType |
HumanData.HandFootType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static HumanData.HandFootType[] |
HumanData.HandFootType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
HumanPosturePredictionBuilder.HandFootCsysData |
HumanPosturePredictionBuilder.getHandFootCsys(HumanData.HandFootType handFoot,
HumanData.SideType side)
Get the Csys of hand foot.
|
NXObject[] |
HumanPosturePredictionBuilder.getHandFootDataCurves(HumanData.HandFootType handFoot,
HumanData.SideType side)
Get the curves or edges of steering wheel or pedal of hand foot data, it will return NULL if the steering wheel pedal type is
not Curve
License requirements: solid_modeling ("SOLIDS MODELING"), ug_human ("Human Modelling") . |
Body[] |
HumanPosturePredictionBuilder.getHandFootDataSolids(HumanData.HandFootType handFoot,
HumanData.SideType side)
Get the solid bodies of steering wheel or pedal of hand foot data, it will return NULL if the steering wheel pedal type
is not Solid
License requirements: solid_modeling ("SOLIDS MODELING"), ug_human ("Human Modelling") . |
HumanPosturePredictionBuilder.SteeringWheelPedalType |
HumanPosturePredictionBuilder.getHandFootDataType(HumanData.HandFootType handFoot,
HumanData.SideType side)
Get the steering wheel and pedal types of hand foot data
License requirements: solid_modeling ("SOLIDS MODELING"), ug_human ("Human Modelling") . |
void |
HumanPosturePredictionBuilder.setHandFootCsys(HumanData.HandFootType handFoot,
HumanData.SideType side,
Point3d position,
Matrix3x3 orientation)
Set the Csys of hand foot, the hand foot csys should be on solid, curve or not conflict with
SAE data related to its steering wheel and pedal type.
|
void |
HumanPosturePredictionBuilder.setHandFootDataCurves(HumanData.HandFootType handFoot,
HumanData.SideType side,
NXObject[] curves)
Set the curves or edges of steering wheel or pedal of hand foot data, the steering wheel pedal type should
be set as Curve and the input curves should be closed
License requirements: solid_modeling ("SOLIDS MODELING"), ug_human ("Human Modelling") . |
void |
HumanPosturePredictionBuilder.setHandFootDataSolids(HumanData.HandFootType handFoot,
HumanData.SideType side,
Body[] solids)
Set the solid bodies of steering wheel or pedal of hand foot data, the steering wheel pedal type should be set as Solid
License requirements: solid_modeling ("SOLIDS MODELING"), ug_human ("Human Modelling") . |
void |
HumanPosturePredictionBuilder.setHandFootDataType(HumanData.HandFootType handFoot,
HumanData.SideType side,
HumanPosturePredictionBuilder.SteeringWheelPedalType steeringWheelPedalType)
Set the steering wheel and pedal types of hand foot data.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.