Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
Modifier and Type | Field and Description |
---|---|
static FlatteningBuilder.FlatteningConstantType |
FlatteningBuilder.FlatteningConstantType.CONSTANT_BODY_VOLUME
force constant volume of the body
|
static FlatteningBuilder.FlatteningConstantType |
FlatteningBuilder.FlatteningConstantType.CONSTANT_CURVE_LENGTH
Force constant length
|
static FlatteningBuilder.FlatteningConstantType |
FlatteningBuilder.FlatteningConstantType.CONSTANT_FACE_AREA
Force constant area
|
static FlatteningBuilder.FlatteningConstantType |
FlatteningBuilder.FlatteningConstantType.NO_CONSTRAINTS
No constraints
|
Modifier and Type | Method and Description |
---|---|
FlatteningBuilder.FlatteningConstantType |
FlatteningBuilder.flatteningConstant()
Deprecated.
Deprecated in NX11.0.0. Use
FlatteningAndFormingBuilder instead.
|
static FlatteningBuilder.FlatteningConstantType |
FlatteningBuilder.FlatteningConstantType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static FlatteningBuilder.FlatteningConstantType |
FlatteningBuilder.FlatteningConstantType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static FlatteningBuilder.FlatteningConstantType[] |
FlatteningBuilder.FlatteningConstantType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
FlatteningBuilder.setFlatteningConstant(FlatteningBuilder.FlatteningConstantType flatteningConstant)
Deprecated.
Deprecated in NX11.0.0. Use
FlatteningAndFormingBuilder instead.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.