Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
nxopen.geometricutilities |
Provides classes and interfaces for Geometric Utilities.
|
Modifier and Type | Method and Description |
---|---|
ExpressionSectionSet |
Part.createEmptyExpressionSectionSet()
Creates an empty ExpressionSectionSet item
License requirements: None. |
ExpressionSectionSet |
Part.createExpressionSectionSet(Section section,
String value,
String unitsType,
int index)
Creates an ExpressionSectionSet item that contains a
Section collection
and a corresponding expression
License requirements: None. |
ExpressionSectionSet |
ExpressionSectionSetList.findItem(int index)
Returns the object at the input index.
|
ExpressionSectionSet[] |
ExpressionSectionSetList.getContents()
Gets the contents of the entire list
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
ExpressionSectionSetList.append(ExpressionSectionSet object)
Appends an object to the list
License requirements: None. |
void |
ExpressionSectionSetList.append(ExpressionSectionSet[] objects)
Appends a set of objects to the list
License requirements: None. |
void |
ExpressionSectionSetList.erase(ExpressionSectionSet obj)
Erases the object from the list, but does not delete the object.
|
void |
ExpressionSectionSetList.erase(ExpressionSectionSet obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
ExpressionSectionSetList.findIndex(ExpressionSectionSet obj)
Finds the index where the input object appears.
|
void |
ExpressionSectionSetList.insert(int location,
ExpressionSectionSet object)
Inserts an object at the specified location
License requirements: None. |
void |
ExpressionSectionSetList.setContents(ExpressionSectionSet[] objects)
Sets the contents of the entire list.
|
void |
ExpressionSectionSetList.swap(ExpressionSectionSet object1,
ExpressionSectionSet object2)
Exchanges the position of two objects inside the list.
|
Modifier and Type | Interface and Description |
---|---|
interface |
TwoExpressionsSectionSet
Represents a two dimension list section item builder
To create a new instance of this class, use Part.createEmptyTwoExpressionsSectionSet() Created in NX9.0.0 |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.