Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
Modifier and Type | Field and Description |
---|---|
static DxfdwgImporter.ImportCurvesAs |
DxfdwgImporter.ImportCurvesAs.CURVES
Convert curves as curves
|
static DxfdwgImporter.ImportCurvesAs |
DxfdwgImporter.ImportCurvesAs.SKETCH_CURVES
Convert curves as sketch curves
|
Modifier and Type | Method and Description |
---|---|
DxfdwgImporter.ImportCurvesAs |
DxfdwgImporter.importCurvesType()
Returns the ImportCurvesType command - When model data is imported on drawing sheet, this can be set in order to sketch a curve or many curves
License requirements: None. |
static DxfdwgImporter.ImportCurvesAs |
DxfdwgImporter.ImportCurvesAs.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DxfdwgImporter.ImportCurvesAs |
DxfdwgImporter.ImportCurvesAs.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DxfdwgImporter.ImportCurvesAs[] |
DxfdwgImporter.ImportCurvesAs.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
DxfdwgImporter.setImportCurvesType(DxfdwgImporter.ImportCurvesAs importCurvesType)
License requirements: None. |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.