Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
Modifier and Type | Field and Description |
---|---|
static DxfdwgImporter.ConvLayoutsAs |
DxfdwgImporter.ConvLayoutsAs.ALL
Convert all layouts
|
static DxfdwgImporter.ConvLayoutsAs |
DxfdwgImporter.ConvLayoutsAs.SELECTED_IN_PREVIEW
Convert selected layouts
|
Modifier and Type | Method and Description |
---|---|
DxfdwgImporter.ConvLayoutsAs |
DxfdwgImporter.convLayouts()
Returns the ConvLayouts command - this will determine if all or selected layouts are translated
License requirements: None. |
static DxfdwgImporter.ConvLayoutsAs |
DxfdwgImporter.ConvLayoutsAs.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DxfdwgImporter.ConvLayoutsAs |
DxfdwgImporter.ConvLayoutsAs.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DxfdwgImporter.ConvLayoutsAs[] |
DxfdwgImporter.ConvLayoutsAs.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
DxfdwgImporter.setConvLayouts(DxfdwgImporter.ConvLayoutsAs convLayoutsAs)
License requirements: None. |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.