Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
Modifier and Type | Field and Description |
---|---|
static DxfdwgCreator.WidthfactorMethodOptions |
DxfdwgCreator.WidthfactorMethodOptions.AUTOMATIC_CALCULATION |
static DxfdwgCreator.WidthfactorMethodOptions |
DxfdwgCreator.WidthfactorMethodOptions.SCALE_NXASPECTRATIO_WITH_SPECIFIED_VALUE |
static DxfdwgCreator.WidthfactorMethodOptions |
DxfdwgCreator.WidthfactorMethodOptions.USE_SAME_AS_NXASPECTRATIO |
static DxfdwgCreator.WidthfactorMethodOptions |
DxfdwgCreator.WidthfactorMethodOptions.USE_VALUE_SPECIFIED_IN_MAPPING_FILE |
Modifier and Type | Method and Description |
---|---|
static DxfdwgCreator.WidthfactorMethodOptions |
DxfdwgCreator.WidthfactorMethodOptions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DxfdwgCreator.WidthfactorMethodOptions |
DxfdwgCreator.WidthfactorMethodOptions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DxfdwgCreator.WidthfactorMethodOptions[] |
DxfdwgCreator.WidthfactorMethodOptions.values()
Returns an array that contains the values for this enum.
|
DxfdwgCreator.WidthfactorMethodOptions |
DxfdwgCreator.widthFactorMode()
Returns the autocad widthfactor calculation method - this will decide the acad widthfactor method to be used.
|
Modifier and Type | Method and Description |
---|---|
void |
DxfdwgCreator.setWidthFactorMode(DxfdwgCreator.WidthfactorMethodOptions widthFactorMode)
License requirements: None. |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.