Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
Modifier and Type | Field and Description |
---|---|
static DxfdwgCreator.ExportScaleOptions |
DxfdwgCreator.ExportScaleOptions.BASE_VIEW
Base View Scale
|
static DxfdwgCreator.ExportScaleOptions |
DxfdwgCreator.ExportScaleOptions.DEFAULT
Default scale(1:1)
|
static DxfdwgCreator.ExportScaleOptions |
DxfdwgCreator.ExportScaleOptions.USER_SPECIFIED
User specified Scale
|
Modifier and Type | Method and Description |
---|---|
DxfdwgCreator.ExportScaleOptions |
DxfdwgCreator.exportScaleOption()
Returns the export scale Options - this will determine if the scale should be used from Default, Base View or User specified
License requirements: None. |
static DxfdwgCreator.ExportScaleOptions |
DxfdwgCreator.ExportScaleOptions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DxfdwgCreator.ExportScaleOptions |
DxfdwgCreator.ExportScaleOptions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DxfdwgCreator.ExportScaleOptions[] |
DxfdwgCreator.ExportScaleOptions.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
DxfdwgCreator.setExportScaleOption(DxfdwgCreator.ExportScaleOptions exportScaleOption)
License requirements: None. |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.