Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
Modifier and Type | Field and Description |
---|---|
static DxfdwgCreator.ExportFromOption |
DxfdwgCreator.ExportFromOption.DISPLAY_PART
export data from displayed part
|
static DxfdwgCreator.ExportFromOption |
DxfdwgCreator.ExportFromOption.EXISTING_PART
export data from existing part which is on disk
|
Modifier and Type | Method and Description |
---|---|
DxfdwgCreator.ExportFromOption |
DxfdwgCreator.exportFrom()
Returns the export from - this option will determine if data from display part or existing part is exported
License requirements: None. |
static DxfdwgCreator.ExportFromOption |
DxfdwgCreator.ExportFromOption.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DxfdwgCreator.ExportFromOption |
DxfdwgCreator.ExportFromOption.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DxfdwgCreator.ExportFromOption[] |
DxfdwgCreator.ExportFromOption.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
DxfdwgCreator.setExportFrom(DxfdwgCreator.ExportFromOption exportFrom)
License requirements: None. |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.