Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
Modifier and Type | Field and Description |
---|---|
static DxfdwgCreator.ExportFacesAsOptions |
DxfdwgCreator.ExportFacesAsOptions.FACETS
export faces as facets
|
static DxfdwgCreator.ExportFacesAsOptions |
DxfdwgCreator.ExportFacesAsOptions.POLYLINE_MESH
export faces as polyline mesh
|
Modifier and Type | Method and Description |
---|---|
DxfdwgCreator.ExportFacesAsOptions |
DxfdwgCreator.exportFacesAs()
Returns the export faces as - this will determine if the faces should be exported as facets or polyline mesh
License requirements: None. |
static DxfdwgCreator.ExportFacesAsOptions |
DxfdwgCreator.ExportFacesAsOptions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DxfdwgCreator.ExportFacesAsOptions |
DxfdwgCreator.ExportFacesAsOptions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DxfdwgCreator.ExportFacesAsOptions[] |
DxfdwgCreator.ExportFacesAsOptions.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
DxfdwgCreator.setExportFacesAs(DxfdwgCreator.ExportFacesAsOptions exportFacesAs)
License requirements: None. |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.