Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
Modifier and Type | Field and Description |
---|---|
static DatumConstraint.Solution |
DatumConstraint.Solution.BINORMAL |
static DatumConstraint.Solution |
DatumConstraint.Solution.NORMAL |
static DatumConstraint.Solution |
DatumConstraint.Solution.OPPOSITE_BINORMAL
Datum axis at opposite to binormal to curve
|
static DatumConstraint.Solution |
DatumConstraint.Solution.OPPOSITE_NORMAL |
static DatumConstraint.Solution |
DatumConstraint.Solution.OPPOSITE_TANGENT |
static DatumConstraint.Solution |
DatumConstraint.Solution.PROJECT
This direction is calculated by projecting a point selected along a curve
to a line, a datum axis, an edge of a solid, a planar face or a datum plane
|
static DatumConstraint.Solution |
DatumConstraint.Solution.TANGENT |
static DatumConstraint.Solution |
DatumConstraint.Solution.UNDEFINED |
Modifier and Type | Method and Description |
---|---|
DatumConstraint.Solution |
DatumConstraint.alternateSolution()
Returns
License requirements: solid_modeling ("SOLIDS MODELING") . |
static DatumConstraint.Solution |
DatumConstraint.Solution.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DatumConstraint.Solution |
DatumConstraint.Solution.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DatumConstraint.Solution[] |
DatumConstraint.Solution.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
DatumConstraint.setAlternateSolution(DatumConstraint.Solution solution)
License requirements: solid_modeling ("SOLIDS MODELING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.