Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
Modifier and Type | Method and Description |
---|---|
DateItemBuilder |
DateBuilder.createDateItemBuilder()
Create a
DateItemBuilder object that can be stored in
the DateItemList. |
DateItemBuilder |
DateBuilder.dateItem()
Returns a
DateItemBuilder object used for simple date and time storage. |
DateItemBuilder |
DateItemBuilderList.findItem(int index)
Returns the object at the input index.
|
DateItemBuilder |
DateBuilder.fromDateItem()
Returns a
DateItemBuilder object used for simple date and time storage. |
DateItemBuilder[] |
DateItemBuilderList.getContents()
Gets the contents of the entire list
License requirements: None. |
DateItemBuilder |
DateBuilder.toDateItem()
Returns a
DateItemBuilder object used for simple date and time storage. |
Modifier and Type | Method and Description |
---|---|
void |
DateItemBuilderList.append(DateItemBuilder object)
Appends an object to the list
License requirements: None. |
void |
DateItemBuilderList.append(DateItemBuilder[] objects)
Appends a set of objects to the list
License requirements: None. |
void |
DateItemBuilderList.erase(DateItemBuilder obj)
Erases the object from the list, but does not delete the object.
|
void |
DateItemBuilderList.erase(DateItemBuilder obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
DateItemBuilderList.findIndex(DateItemBuilder obj)
Finds the index where the input object appears.
|
void |
DateItemBuilderList.insert(int location,
DateItemBuilder object)
Inserts an object at the specified location
License requirements: None. |
void |
DateItemBuilderList.setContents(DateItemBuilder[] objects)
Sets the contents of the entire list.
|
void |
DateItemBuilderList.swap(DateItemBuilder object1,
DateItemBuilder object2)
Exchanges the position of two objects inside the list.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.