Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
Modifier and Type | Field and Description |
---|---|
static BasePart.PartPreview |
BasePart.PartPreview.NONE
No preview image is stored for the part.
|
static BasePart.PartPreview |
BasePart.PartPreview.ON_DEMAND
Create a preview image on demand.
|
static BasePart.PartPreview |
BasePart.PartPreview.ON_SAVE
Create a preview image when the part is saved.
|
Modifier and Type | Method and Description |
---|---|
BasePart.PartPreview |
BasePart.partPreviewMode()
Returns the preview mode
License requirements: None. |
static BasePart.PartPreview |
BasePart.PartPreview.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static BasePart.PartPreview |
BasePart.PartPreview.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static BasePart.PartPreview[] |
BasePart.PartPreview.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
BasePart.setPartPreviewMode(BasePart.PartPreview mode)
Sets the preview mode
License requirements: None. |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.