Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
nxopen.gateway |
Provides classes and interfaces for Gateway.
|
Modifier and Type | Field and Description |
---|---|
static BasePart.BookmarkOption |
BasePart.BookmarkOption.ALL
Write component groups, load options and structure.
|
static BasePart.BookmarkOption |
BasePart.BookmarkOption.ALL_PLUS_DISPLAY
Write component groups, load options, structure and display attributes
|
static BasePart.BookmarkOption |
BasePart.BookmarkOption.COMPONENT_GROUPS_LOAD_OPTIONS
Write component groups and load options.
|
static BasePart.BookmarkOption |
BasePart.BookmarkOption.COMPONENT_GROUPS_LOAD_OPTIONS_PLUS_DISPLAY
Write component groups, load options and display attributes
|
static BasePart.BookmarkOption |
BasePart.BookmarkOption.COMPONENT_GROUPS_ONLY
Write component groups only.
|
static BasePart.BookmarkOption |
BasePart.BookmarkOption.COMPONENT_GROUPS_ONLY_PLUS_DISPLAY
Write component groups and display attributes
|
static BasePart.BookmarkOption |
BasePart.BookmarkOption.DISPLAY_ONLY
Write only display attributes
|
static BasePart.BookmarkOption |
BasePart.BookmarkOption.EMPTY
Write nothing but header information
|
Modifier and Type | Method and Description |
---|---|
static BasePart.BookmarkOption |
BasePart.BookmarkOption.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static BasePart.BookmarkOption |
BasePart.BookmarkOption.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static BasePart.BookmarkOption[] |
BasePart.BookmarkOption.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
BasePart.saveBookmark(String fileName,
BasePart.BookmarkOption option)
Saves a bookmark file.
|
Modifier and Type | Method and Description |
---|---|
void |
BookmarkFile.saveWithDescription(String pathName,
BasePart.BookmarkOption bookmarkOption,
String description)
Creates a bookmark file including a description.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.