Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
Modifier and Type | Field and Description |
---|---|
static AutomaticTraceline.ModeOption |
AutomaticTraceline.ModeOption.EVALUATE
Evaluate which mode to use
|
static AutomaticTraceline.ModeOption |
AutomaticTraceline.ModeOption.INFER
Infer orientation from start and end directions
|
static AutomaticTraceline.ModeOption |
AutomaticTraceline.ModeOption.ORIENTATION
Align with orientation
|
Modifier and Type | Method and Description |
---|---|
AutomaticTraceline.ModeOption |
AutomaticTraceline.mode()
Returns the mode of the traceline
License requirements: assemblies ("ASSEMBLIES MODULE") . |
static AutomaticTraceline.ModeOption |
AutomaticTraceline.ModeOption.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static AutomaticTraceline.ModeOption |
AutomaticTraceline.ModeOption.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static AutomaticTraceline.ModeOption[] |
AutomaticTraceline.ModeOption.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
AutomaticTraceline |
TracelineCollection.createAutomaticTraceline(Explosion explosion,
Point startPoint,
Direction startDirection,
Point endPoint,
Direction endDirection,
Matrix3x3 orientation,
AutomaticTraceline.ModeOption mode,
int solution,
double startOffset,
double endOffset,
int[] segmentIndices,
double[] segmentLengths)
Create an automatic traceline
License requirements: assemblies ("ASSEMBLIES MODULE") . |
void |
AutomaticTraceline.setMode(AutomaticTraceline.ModeOption mode)
License requirements: assemblies ("ASSEMBLIES MODULE") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.