Package | Description |
---|---|
nxopen.cae.xyplot |
Provides classes and interfaces for XY Graphing.
|
Modifier and Type | Field and Description |
---|---|
static UnitSystem |
UnitSystem.CUSTOM
Deprecated.
Custom unit
|
static UnitSystem |
UnitSystem.FUNCTION
Deprecated.
Function unit
|
static UnitSystem |
UnitSystem.IN
Deprecated.
Inch unit
|
static UnitSystem |
UnitSystem.MM
Deprecated.
Millimeter unit
|
static UnitSystem |
UnitSystem.MN
Deprecated.
Milliforce unit
|
static UnitSystem |
UnitSystem.MODEL
Deprecated.
Model unit
|
static UnitSystem |
UnitSystem.SI
Deprecated.
International standard unit
|
Modifier and Type | Method and Description |
---|---|
UnitSystem |
AxisStyleSetting.unitSystem()
Deprecated.
Deprecated in NX12.0.0. Use
AxisStyleSetting.unitSystemType() instead.
|
static UnitSystem |
UnitSystem.valueOf(int value)
Deprecated.
Returns the enum constant of the specified enum type with the specified value.
|
static UnitSystem |
UnitSystem.valueOf(String name)
Deprecated.
Returns the enum constant of the specified enum type with the specified name.
|
static UnitSystem[] |
UnitSystem.values()
Deprecated.
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
AxisStyleSetting.setUnitSystem(UnitSystem unitSystem)
Deprecated.
Deprecated in NX12.0.0. Use
AxisStyleSetting.setUnitSystemType(nxopen.cae.XyFunctionUnitSystem) instead.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.