Package | Description |
---|---|
nxopen.cae.xyplot |
Provides classes and interfaces for XY Graphing.
|
Modifier and Type | Field and Description |
---|---|
static Preference.TargetGraphicWindowOption |
Preference.TargetGraphicWindowOption.BOTH
Shows plot graph on either main graphic window or a separate graphic window
|
static Preference.TargetGraphicWindowOption |
Preference.TargetGraphicWindowOption.MAIN
Only shows plot graph on main graphic window
|
static Preference.TargetGraphicWindowOption |
Preference.TargetGraphicWindowOption.SEPARATE
Only shows plot graph on a separate graphic window
|
Modifier and Type | Method and Description |
---|---|
Preference.TargetGraphicWindowOption |
Preference.targetWindowSetting()
Returns the target window setting value
License requirements: None. |
static Preference.TargetGraphicWindowOption |
Preference.TargetGraphicWindowOption.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static Preference.TargetGraphicWindowOption |
Preference.TargetGraphicWindowOption.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static Preference.TargetGraphicWindowOption[] |
Preference.TargetGraphicWindowOption.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
Preference.setTargetWindowSetting(Preference.TargetGraphicWindowOption targetWindowSetting)
License requirements: None. |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.