Package | Description |
---|---|
nxopen.cae.xyplot |
Provides classes and interfaces for XY Graphing.
|
Modifier and Type | Field and Description |
---|---|
static Direction |
Direction.X
Option to show plot in the X axis direction
|
static Direction |
Direction.XZ
Option to show plot in the both X and Z axis direction
|
static Direction |
Direction.Z
Option to show plot in the Z axis direction
|
Modifier and Type | Method and Description |
---|---|
Direction |
PlateStyle3DSetting.direction()
Deprecated.
Deprecated in NX12.0.0. There is no replacement for this class.
|
Direction |
LineStyle3DSetting.direction()
Returns the line direction
License requirements: None. |
static Direction |
Direction.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static Direction |
Direction.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static Direction[] |
Direction.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
PlateStyle3DSetting.setDirection(Direction direction)
Deprecated.
Deprecated in NX12.0.0. There is no replacement for this class.
|
void |
LineStyle3DSetting.setDirection(Direction direction)
License requirements: None. |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.