Package | Description |
---|---|
nxopen.cae.xyplot |
Provides classes and interfaces for XY Graphing.
|
Modifier and Type | Field and Description |
---|---|
static ContouringRange |
ContouringRange.BORDER_GRID
Option to show contour range on the border of the grid
|
static ContouringRange |
ContouringRange.FULL_GRID
Option to show contour range on the face of the grid
|
Modifier and Type | Method and Description |
---|---|
ContouringRange |
BaseGridLayoutStyleSetting.contouringRange()
Returns the option to show contour range either on the border or the faces of the grid.
|
static ContouringRange |
ContouringRange.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ContouringRange |
ContouringRange.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ContouringRange[] |
ContouringRange.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
BaseGridLayoutStyleSetting.setContouringRange(ContouringRange contouringRange)
License requirements: None. |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.