public class LegendTablePositionType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_DOCKED
The position of legend table is fixed
|
static int |
_FLOATING
The position of legend table can be dragged
|
static LegendTablePositionType |
DOCKED
The position of legend table is fixed
|
static LegendTablePositionType |
FLOATING
The position of legend table can be dragged
|
Modifier and Type | Method and Description |
---|---|
static LegendTablePositionType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static LegendTablePositionType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static LegendTablePositionType[] |
values()
Returns an array that contains the values for this enum.
|
public static final LegendTablePositionType FLOATING
public static final LegendTablePositionType DOCKED
public static final int _FLOATING
public static final int _DOCKED
public static LegendTablePositionType valueOf(int value)
public static LegendTablePositionType valueOf(String name)
public static LegendTablePositionType[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.