Package | Description |
---|---|
nxopen.cae.optimization |
Provides classes and interfaces relating to Optimization.
|
Modifier and Type | Field and Description |
---|---|
static TBSTopologySensitivityOptimizationParameters.MaterialInterpolation |
TBSTopologySensitivityOptimizationParameters.MaterialInterpolation.RAMP
Rational approximation of material properties
|
static TBSTopologySensitivityOptimizationParameters.MaterialInterpolation |
TBSTopologySensitivityOptimizationParameters.MaterialInterpolation.SIMP
Solid Isotropic material with penalization
|
Modifier and Type | Method and Description |
---|---|
TBSTopologySensitivityOptimizationParameters.MaterialInterpolation |
TBSTopologySensitivityOptimizationParameters.materialInterpolationOption()
Returns the material interpolation scheme
License requirements: None. |
static TBSTopologySensitivityOptimizationParameters.MaterialInterpolation |
TBSTopologySensitivityOptimizationParameters.MaterialInterpolation.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TBSTopologySensitivityOptimizationParameters.MaterialInterpolation |
TBSTopologySensitivityOptimizationParameters.MaterialInterpolation.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TBSTopologySensitivityOptimizationParameters.MaterialInterpolation[] |
TBSTopologySensitivityOptimizationParameters.MaterialInterpolation.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
TBSTopologySensitivityOptimizationParameters.setMaterialInterpolationOption(TBSTopologySensitivityOptimizationParameters.MaterialInterpolation materialInterpolationOption)
License requirements: cae_opt_topo ("NX Topology Optimization") OR cae_opt_topobead ("NX Bead Optimization") OR cae_opt_toposhape ("NX Shape Optimization") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.