Package | Description |
---|---|
nxopen.cae.optimization |
Provides classes and interfaces relating to Optimization.
|
Modifier and Type | Field and Description |
---|---|
static TBSTopologyLinkCondition.SymmetryOption |
TBSTopologyLinkCondition.SymmetryOption.CYCLIC_SYMMETRY
Cyclic symmetry definition
|
static TBSTopologyLinkCondition.SymmetryOption |
TBSTopologyLinkCondition.SymmetryOption.PLANE_SYMMETRY
Plane symmetry referring to the plane which lies
perpendicular to the given axis of the coordinate system
|
Modifier and Type | Method and Description |
---|---|
TBSTopologyLinkCondition.SymmetryOption |
TBSTopologyLinkCondition.symmetryType()
Returns the symmetry link condition type
License requirements: None. |
static TBSTopologyLinkCondition.SymmetryOption |
TBSTopologyLinkCondition.SymmetryOption.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TBSTopologyLinkCondition.SymmetryOption |
TBSTopologyLinkCondition.SymmetryOption.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TBSTopologyLinkCondition.SymmetryOption[] |
TBSTopologyLinkCondition.SymmetryOption.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
TBSTopologyLinkCondition.setSymmetryType(TBSTopologyLinkCondition.SymmetryOption symmetryType)
License requirements: cae_opt_topo ("NX Topology Optimization") OR cae_opt_topobead ("NX Bead Optimization") OR cae_opt_toposhape ("NX Shape Optimization") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.