Package | Description |
---|---|
nxopen.cae.optimization |
Provides classes and interfaces relating to Optimization.
|
Modifier and Type | Field and Description |
---|---|
static TBSTopologyControllerOptimizationParameters.VolumeDefinitionMethod |
TBSTopologyControllerOptimizationParameters.VolumeDefinitionMethod.ABSOLUTE
Specifying the absolute volume
|
static TBSTopologyControllerOptimizationParameters.VolumeDefinitionMethod |
TBSTopologyControllerOptimizationParameters.VolumeDefinitionMethod.PERCENT
Specifying the volume in percentage
|
Modifier and Type | Method and Description |
---|---|
static TBSTopologyControllerOptimizationParameters.VolumeDefinitionMethod |
TBSTopologyControllerOptimizationParameters.VolumeDefinitionMethod.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TBSTopologyControllerOptimizationParameters.VolumeDefinitionMethod |
TBSTopologyControllerOptimizationParameters.VolumeDefinitionMethod.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TBSTopologyControllerOptimizationParameters.VolumeDefinitionMethod[] |
TBSTopologyControllerOptimizationParameters.VolumeDefinitionMethod.values()
Returns an array that contains the values for this enum.
|
TBSTopologyControllerOptimizationParameters.VolumeDefinitionMethod |
TBSTopologyControllerOptimizationParameters.volumeDefinitionOption()
Returns the volume definition option
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
TBSTopologyControllerOptimizationParameters.setVolumeDefinitionOption(TBSTopologyControllerOptimizationParameters.VolumeDefinitionMethod volumeDefinitionOption)
License requirements: cae_opt_topo ("NX Topology Optimization") OR cae_opt_topobead ("NX Bead Optimization") OR cae_opt_toposhape ("NX Shape Optimization") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.