Package | Description |
---|---|
nxopen.cae.optimization |
Provides classes and interfaces relating to Optimization.
|
Modifier and Type | Field and Description |
---|---|
static TBSTopologyControllerOptimizationParameters.AutoFrozen |
TBSTopologyControllerOptimizationParameters.AutoFrozen.BOTH
All loaded elements, elements with load nodes with boundary conditions are excluded from the optimization
|
static TBSTopologyControllerOptimizationParameters.AutoFrozen |
TBSTopologyControllerOptimizationParameters.AutoFrozen.LOAD
All loaded elements and nodes are excluded from the optimization
|
static TBSTopologyControllerOptimizationParameters.AutoFrozen |
TBSTopologyControllerOptimizationParameters.AutoFrozen.OFF
Loaded elements are optimizable
|
static TBSTopologyControllerOptimizationParameters.AutoFrozen |
TBSTopologyControllerOptimizationParameters.AutoFrozen.SPC
Elements with boundary conditions are excluded from the optimization
|
Modifier and Type | Method and Description |
---|---|
TBSTopologyControllerOptimizationParameters.AutoFrozen |
TBSTopologyControllerOptimizationParameters.automaticFrozenOption()
Returns the automatic frozen option
License requirements: None. |
static TBSTopologyControllerOptimizationParameters.AutoFrozen |
TBSTopologyControllerOptimizationParameters.AutoFrozen.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TBSTopologyControllerOptimizationParameters.AutoFrozen |
TBSTopologyControllerOptimizationParameters.AutoFrozen.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TBSTopologyControllerOptimizationParameters.AutoFrozen[] |
TBSTopologyControllerOptimizationParameters.AutoFrozen.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
TBSTopologyControllerOptimizationParameters.setAutomaticFrozenOption(TBSTopologyControllerOptimizationParameters.AutoFrozen autoFrozen)
License requirements: cae_opt_topo ("NX Topology Optimization") OR cae_opt_topobead ("NX Bead Optimization") OR cae_opt_toposhape ("NX Shape Optimization") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.