Package | Description |
---|---|
nxopen.cae.optimization |
Provides classes and interfaces relating to Optimization.
|
Modifier and Type | Field and Description |
---|---|
static TBSTestFunction.Direction |
TBSTestFunction.Direction.GROW
Standard growth
|
static TBSTestFunction.Direction |
TBSTestFunction.Direction.RANDOM
Non-standard nodal random displacement
|
static TBSTestFunction.Direction |
TBSTestFunction.Direction.SHRINK
Standard Shrinkage
|
Modifier and Type | Method and Description |
---|---|
TBSTestFunction.Direction |
TBSTestFunction.testDirectionOption()
Returns the direction of test displacements
License requirements: None. |
static TBSTestFunction.Direction |
TBSTestFunction.Direction.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TBSTestFunction.Direction |
TBSTestFunction.Direction.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TBSTestFunction.Direction[] |
TBSTestFunction.Direction.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
TBSTestFunction.setTestDirectionOption(TBSTestFunction.Direction direction)
License requirements: cae_opt_topobead ("NX Bead Optimization") OR cae_opt_toposhape ("NX Shape Optimization") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.