Package | Description |
---|---|
nxopen.cae.optimization |
Provides classes and interfaces relating to Optimization.
|
Modifier and Type | Field and Description |
---|---|
static TBSSmoothBuilder.SelfIntersectionCheckingOption |
TBSSmoothBuilder.SelfIntersectionCheckingOption.CHECK
Check once
|
static TBSSmoothBuilder.SelfIntersectionCheckingOption |
TBSSmoothBuilder.SelfIntersectionCheckingOption.ITERATIVE
First run without check, then rerun if self-intersections are found
|
static TBSSmoothBuilder.SelfIntersectionCheckingOption |
TBSSmoothBuilder.SelfIntersectionCheckingOption.OFF
No checks
|
static TBSSmoothBuilder.SelfIntersectionCheckingOption |
TBSSmoothBuilder.SelfIntersectionCheckingOption.RUNTIME
Check always
|
Modifier and Type | Method and Description |
---|---|
TBSSmoothBuilder.SelfIntersectionCheckingOption |
TBSSmoothBuilder.selfIntersectionChecking()
Returns the option of self-intersection checking
License requirements: None. |
static TBSSmoothBuilder.SelfIntersectionCheckingOption |
TBSSmoothBuilder.SelfIntersectionCheckingOption.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TBSSmoothBuilder.SelfIntersectionCheckingOption |
TBSSmoothBuilder.SelfIntersectionCheckingOption.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TBSSmoothBuilder.SelfIntersectionCheckingOption[] |
TBSSmoothBuilder.SelfIntersectionCheckingOption.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
TBSSmoothBuilder.setSelfIntersectionChecking(TBSSmoothBuilder.SelfIntersectionCheckingOption selfIntersectionChecking)
License requirements: cae_opt_topo ("NX Topology Optimization") OR cae_opt_topobead ("NX Bead Optimization") OR cae_opt_toposhape ("NX Shape Optimization") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.