Package | Description |
---|---|
nxopen.cae.optimization |
Provides classes and interfaces relating to Optimization.
|
Modifier and Type | Field and Description |
---|---|
static TBSSmoothBuilder.ResultFiltering |
TBSSmoothBuilder.ResultFiltering.FULL
Filters the element material values fully
|
static TBSSmoothBuilder.ResultFiltering |
TBSSmoothBuilder.ResultFiltering.MODERATE
Filters the element material values partially
|
static TBSSmoothBuilder.ResultFiltering |
TBSSmoothBuilder.ResultFiltering.OFF
Don't filter the element material values
|
Modifier and Type | Method and Description |
---|---|
TBSSmoothBuilder.ResultFiltering |
TBSSmoothBuilder.resultFilteringOption()
Returns the result filtering option
License requirements: None. |
static TBSSmoothBuilder.ResultFiltering |
TBSSmoothBuilder.ResultFiltering.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TBSSmoothBuilder.ResultFiltering |
TBSSmoothBuilder.ResultFiltering.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TBSSmoothBuilder.ResultFiltering[] |
TBSSmoothBuilder.ResultFiltering.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
TBSSmoothBuilder.setResultFilteringOption(TBSSmoothBuilder.ResultFiltering resultFilteringOption)
License requirements: cae_opt_topo ("NX Topology Optimization") OR cae_opt_topobead ("NX Bead Optimization") OR cae_opt_toposhape ("NX Shape Optimization") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.