Package | Description |
---|---|
nxopen.cae.optimization |
Provides classes and interfaces relating to Optimization.
|
Modifier and Type | Field and Description |
---|---|
static TBSSmoothBuilder.OriginalSurfaceSmoothingOption |
TBSSmoothBuilder.OriginalSurfaceSmoothingOption.FULL
Allows any modifications to the original surface
|
static TBSSmoothBuilder.OriginalSurfaceSmoothingOption |
TBSSmoothBuilder.OriginalSurfaceSmoothingOption.OFF
No changes to the original surface
|
static TBSSmoothBuilder.OriginalSurfaceSmoothingOption |
TBSSmoothBuilder.OriginalSurfaceSmoothingOption.SHRINK
Allows the nodes on original surface to be moved towards the inside only
|
Modifier and Type | Method and Description |
---|---|
TBSSmoothBuilder.OriginalSurfaceSmoothingOption |
TBSSmoothBuilder.originalSurfaceSmooth()
Returns the option of how to smooth the original surface
License requirements: None. |
static TBSSmoothBuilder.OriginalSurfaceSmoothingOption |
TBSSmoothBuilder.OriginalSurfaceSmoothingOption.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TBSSmoothBuilder.OriginalSurfaceSmoothingOption |
TBSSmoothBuilder.OriginalSurfaceSmoothingOption.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TBSSmoothBuilder.OriginalSurfaceSmoothingOption[] |
TBSSmoothBuilder.OriginalSurfaceSmoothingOption.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
TBSSmoothBuilder.setOriginalSurfaceSmooth(TBSSmoothBuilder.OriginalSurfaceSmoothingOption originalSurfaceSmooth)
License requirements: cae_opt_topo ("NX Topology Optimization") OR cae_opt_topobead ("NX Bead Optimization") OR cae_opt_toposhape ("NX Shape Optimization") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.