Package | Description |
---|---|
nxopen.cae.optimization |
Provides classes and interfaces relating to Optimization.
|
Modifier and Type | Field and Description |
---|---|
static TBSSmoothBuilder.Format |
TBSSmoothBuilder.Format.BDF
Represents surfaces in .bdf file
|
static TBSSmoothBuilder.Format |
TBSSmoothBuilder.Format.IGES
Represents surfaces in .igs file
|
static TBSSmoothBuilder.Format |
TBSSmoothBuilder.Format.STL
Represents surfaces in .stl file
|
Modifier and Type | Method and Description |
---|---|
TBSSmoothBuilder.Format[] |
TBSSmoothBuilder.getFormatOption()
The output result format accessor
License requirements: None. |
static TBSSmoothBuilder.Format |
TBSSmoothBuilder.Format.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TBSSmoothBuilder.Format |
TBSSmoothBuilder.Format.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TBSSmoothBuilder.Format[] |
TBSSmoothBuilder.Format.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
TBSSmoothBuilder.setFormatOption(TBSSmoothBuilder.Format[] formatOption)
The output result format mutator
License requirements: cae_opt_topo ("NX Topology Optimization") OR cae_opt_topobead ("NX Bead Optimization") OR cae_opt_toposhape ("NX Shape Optimization") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.