Package | Description |
---|---|
nxopen.cae.optimization |
Provides classes and interfaces relating to Optimization.
|
Modifier and Type | Field and Description |
---|---|
static TBSShapeLinkCondition.ManufacturingOption |
TBSShapeLinkCondition.ManufacturingOption.PLANE_SYMMETRY
Plane symmetry referring to the plane which lies
perpendicular to the given axis of the coordinate system
|
static TBSShapeLinkCondition.ManufacturingOption |
TBSShapeLinkCondition.ManufacturingOption.ROTATION_SYMMETRY
Rotation symmetry definition
|
static TBSShapeLinkCondition.ManufacturingOption |
TBSShapeLinkCondition.ManufacturingOption.SURFACE_DEMOLD
Demold surface definition
|
static TBSShapeLinkCondition.ManufacturingOption |
TBSShapeLinkCondition.ManufacturingOption.SURFACE_DRILL
Drillable surface definition
|
static TBSShapeLinkCondition.ManufacturingOption |
TBSShapeLinkCondition.ManufacturingOption.SURFACE_STAMP
Stampable surface definition
|
static TBSShapeLinkCondition.ManufacturingOption |
TBSShapeLinkCondition.ManufacturingOption.SURFACE_TURN
Turnable surface definition
|
Modifier and Type | Method and Description |
---|---|
TBSShapeLinkCondition.ManufacturingOption |
TBSShapeLinkCondition.manufacturingType()
Returns the manufacturing type
License requirements: None. |
static TBSShapeLinkCondition.ManufacturingOption |
TBSShapeLinkCondition.ManufacturingOption.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TBSShapeLinkCondition.ManufacturingOption |
TBSShapeLinkCondition.ManufacturingOption.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TBSShapeLinkCondition.ManufacturingOption[] |
TBSShapeLinkCondition.ManufacturingOption.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
TBSShapeLinkCondition.setManufacturingType(TBSShapeLinkCondition.ManufacturingOption manufacturingType)
License requirements: cae_opt_toposhape ("NX Shape Optimization") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.