Package | Description |
---|---|
nxopen.cae.optimization |
Provides classes and interfaces relating to Optimization.
|
Modifier and Type | Field and Description |
---|---|
static TBSOptimizationSolutionBuilder.StrategyType |
TBSOptimizationSolutionBuilder.StrategyType.CONTROLLER
uses controller strategy to run optimization
|
static TBSOptimizationSolutionBuilder.StrategyType |
TBSOptimizationSolutionBuilder.StrategyType.SENSITIVITY
Uses sensitivity strategy to run optimization
|
Modifier and Type | Method and Description |
---|---|
TBSOptimizationSolutionBuilder.StrategyType |
TBSOptimizationSolutionBuilder.strategy()
Returns the optimization strategy
License requirements: None. |
static TBSOptimizationSolutionBuilder.StrategyType |
TBSOptimizationSolutionBuilder.StrategyType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TBSOptimizationSolutionBuilder.StrategyType |
TBSOptimizationSolutionBuilder.StrategyType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TBSOptimizationSolutionBuilder.StrategyType[] |
TBSOptimizationSolutionBuilder.StrategyType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
TBSOptimizationSolutionBuilder.setStrategy(TBSOptimizationSolutionBuilder.StrategyType strategy)
License requirements: cae_opt_topo ("NX Topology Optimization") OR cae_opt_topobead ("NX Bead Optimization") OR cae_opt_toposhape ("NX Shape Optimization") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.