Package | Description |
---|---|
nxopen.cae.optimization |
Provides classes and interfaces relating to Optimization.
|
Modifier and Type | Field and Description |
---|---|
static TBSLoadCaseManager.SelectionType |
TBSLoadCaseManager.SelectionType.MAXIMUM
Maximum value of the selected load cases
|
static TBSLoadCaseManager.SelectionType |
TBSLoadCaseManager.SelectionType.MINIMUM
Minimum value of the selected load cases
|
static TBSLoadCaseManager.SelectionType |
TBSLoadCaseManager.SelectionType.SUM
Sum of the selected load cases
|
Modifier and Type | Method and Description |
---|---|
TBSLoadCaseManager.SelectionType |
TBSLoadCaseManager.selectionOption()
Returns the selection option
License requirements: None. |
static TBSLoadCaseManager.SelectionType |
TBSLoadCaseManager.SelectionType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TBSLoadCaseManager.SelectionType |
TBSLoadCaseManager.SelectionType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TBSLoadCaseManager.SelectionType[] |
TBSLoadCaseManager.SelectionType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
TBSLoadCaseManager.setSelectionOption(TBSLoadCaseManager.SelectionType selectionOption)
License requirements: cae_opt_topo ("NX Topology Optimization") OR cae_opt_topobead ("NX Bead Optimization") OR cae_opt_toposhape ("NX Shape Optimization") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.