Package | Description |
---|---|
nxopen.cae.optimization |
Provides classes and interfaces relating to Optimization.
|
Modifier and Type | Field and Description |
---|---|
static TBSGroupDefinition.GroupElementType |
TBSGroupDefinition.GroupElementType.ELEMENT
The group contains element
|
static TBSGroupDefinition.GroupElementType |
TBSGroupDefinition.GroupElementType.NODE
The group contains node
|
Modifier and Type | Method and Description |
---|---|
TBSGroupDefinition.GroupElementType |
TBSGroupDefinition.getElementType()
Returns the group element type
License requirements: None. |
TBSGroupDefinition.GroupElementType |
TBSBaseDesignVariableBuilder.selectionAreaType()
Returns the type of selection location on which design variable is applied
License requirements: None. |
static TBSGroupDefinition.GroupElementType |
TBSGroupDefinition.GroupElementType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TBSGroupDefinition.GroupElementType |
TBSGroupDefinition.GroupElementType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TBSGroupDefinition.GroupElementType[] |
TBSGroupDefinition.GroupElementType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
TBSBaseDesignVariableBuilder.setSelectionAreaType(TBSGroupDefinition.GroupElementType areaType)
License requirements: cae_opt_topo ("NX Topology Optimization") OR cae_opt_topobead ("NX Bead Optimization") OR cae_opt_toposhape ("NX Shape Optimization") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.